NX
Parts list contains [...] in the PC No column with no manual text
2022-03-09T13:14:52Z
NX for Design
Summary
Details
Parts list contains [...] in the PC No column with no manual text
Solution
The parts list uses the Callout component instance value in the PC NO column. If there are several instances of the component in the assembly, and they have different values for this attribute, the [...] will appear in the cell. One way to fix this is to use Bulk Edit in the component properties and change the values manually to be the same which will result in the specified callout value and quantity of the component in a single line in the parts list. Another way to fix this is to clear the syntax in the Attribute Name field and inserting $~C into the Default Text field of the Parts List setting dialog as seen below.
Notes and References
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: DRAFTING Version: V2008 Function: TABLES